2/8/2018 7:17 PM | |
Posts: 8 Rating: (0) |
Here are some images of a converter that makes me a problem
Attachmentconverter.zip (312 Downloads) |
Last edited by: Jen_Moderator at: 2/9/2018 10:54:26 AMAdded all images as an attachment. |
|
2/20/2018 9:04 PM | |
Posts: 8 Rating: (0) |
Respect my friends ... the situation is the following ... when I start the machine on the v110 diode there is a voltage of 23.8 DC of the power board itself and regulation there is a voltage of 5,12 and 24 volts DC ..... 6SE7031-7HG84-1JA1 ... . I demounted the complete CUVC and measured the voltages I got the approximate value of the elements by the datasheet, only the power supply of the elements was correct ... I wasted the EEPROM at the positions D14 and D16 I approach .... I oscilloscope I followed the magistrale on the board .... signals from FLASH I'm not correct ... full harmonicsAM29F200B-70EC ...... and the signal on the transistor V1 is deformed ... I will try to replace the new EEPROM and I will report ..
AttachmentAtlasCopco GA50VSD ff.zip (280 Downloads) |
Last edited by: munja2 at: 2/20/2018 10:24:49 PM |
|
2/20/2018 9:07 PM | |
Posts: 8 Rating: (0) |
oscillograms from the board CUVC
AttachmentCUVC.zip (348 Downloads) |
3/9/2018 10:08 AM | |
Joined: 3/25/2008 Last visit: 9/20/2024 Posts: 193 Rating: (8) |
what exactly is it about? the X9 terminal 4 and 5 is the cooling fan shutdown delay.
|
6/2/2018 1:03 AM | |
Posts: 25 Rating: (1) |
|
Follow us on