7/18/2017 12:33 PM | |
Posts: 2 Rating: (0) |
Good day. Write through the translator I have the controller PXC001.E.D and the reverse osmosis controller CCT 8320. I want to read data from the controller, reverse osmosis system, 2 separate status byte. Next, we must expand the status byte bits. How to take bytes in PXC001.E.D? The functions BI and AI is not fit for service. If this feature MI? How to set the ModBus address of the variable? AttachmentCCT8320.pdf (525 Downloads) |
7/23/2017 11:27 PM | |
Joined: 4/28/2015 Last visit: 6/15/2023 Posts: 1 Rating: (0) |
ESTOY CON UN TEMA MUY SIMILAR...TAMBIÉN NECESITO LA MISMA AYUDA.... |
Follow us on