3/19/2018 9:04 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Hello, very important question, what full OS version on PC? |
With best regards... |
|
3/19/2018 9:26 AM | |
Joined: 1/18/2008 Last visit: 3/20/2024 Posts: 36 Rating: (0) |
Hi What are your PG/PC interface settings? What speed setting is selected on the PG/PC adapter? Regards Andrew |
3/19/2018 11:25 AM | |
Posts: 4 Rating: (1) |
Hi, Thanks for your advice. I zipped and attached what I already have. I will visit my client at Thursday and try handle this. You mean the issue can be beacuse I using VM? Little Bit explanaiton For MPI page network parameters I used 187.5 Kbps as well and It didnt helped. For local connection page I used transmision rate I used 19200 and 38400 following to small switch on adapter. I used COM1 and COM2 but didint worked.
AttachmentErrors.zip (61 Downloads) |
3/19/2018 1:57 PM | |
Posts: 4 Rating: (1) |
I will remmber do it on Thrusday morning. oght now Im 120km away from this PLC. I will back to this |
Follow us on