3/19/2018 10:54 AM | |
Joined: 7/23/2016 Last visit: 2/18/2024 Posts: 37 Rating: (0) |
dear all could any one help me i have a problem in one D425 CPU , it doesn't working normally and the notification LEDs as showing in the photo RDY is green DPT is green but the others are off , and the seven segment is showing number 6 in my machine there is different status as the following RDY , RUN , DP1 , DP2 all are green and the others are off , and the seven segment is showing number 6 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/20/2018 11:27:07 AMNew subject after splitting Ahmed Atef |
|
3/19/2018 2:41 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22228 Rating: (2980)
|
hello, try it with ethernet. is more easy then profibus or mpi. regards christoph |
Follow us on