3/20/2018 8:02 AM | |
Posts: 305 Rating: (2) |
can you config a example give me test ,i think it is fast idea . eveytime is not right.... |
Last edited by: TechWing at: 3/20/2018 8:34:56 AM |
|
3/20/2018 1:39 PM | |
Posts: 305 Rating: (2) |
hello.i config the funtion to download ,but program has any command ,the D425 can runnng ,program is blank ,D425 can running ,what is wrong ? |
3/20/2018 3:21 PM | |
Posts: 305 Rating: (2) |
use telegram 106 is right ? enable extenal encoder ,r482 not data . |
3/20/2018 4:16 PM | |
Joined: 5/12/2006 Last visit: 9/23/2024 Posts: 22369 Rating: (3012)
|
Hello, no telegram 106 is wrong. Do you have a encoder created so that you can use this commands?
Christoph |
3/21/2018 5:28 AM | |
Joined: 5/12/2006 Last visit: 9/23/2024 Posts: 22369 Rating: (3012)
|
whcih to is configured for the dataexchange in simotion with the drive? |
3/21/2018 7:20 AM | |
Posts: 305 Rating: (2) |
now can connect encoder ,at sinamics read positon data. TO connect it ,can't enable extenalencoder. how can setup TO parameter with SSI... |
3/21/2018 7:31 AM | |
Posts: 305 Rating: (2) |
upload sinamics ? i change TO parameter ,download,the D425 can't change . |
Last edited by: TechWing at: 3/21/2018 7:33:32 AM |
|
Follow us on