12/9/2020 10:56 AM | |
Joined: 8/29/2019 Last visit: 4/24/2024 Posts: 33 Rating: (0) |
Hello, any news on the event "System initiated session termination" 16# 02:4427? |
3/23/2023 12:06 PM | |
Joined: 8/3/2009 Last visit: 5/8/2024 Posts: 12909 Rating: (1646)
|
Hello Simousss85 The Error means that the HMI has terminated the connection (not the PLC) -> If you cannot get the connection work at all then an issue could be this: https://support.industry.siemens.com/cs/ww/en/view/109803668 If the connection works and randomly disconnects with this error then it could also be that the Panel is in an overload and cannot handle the communication again... -> Does it work after a reboot? which Image Version do you use on the Panel? FW version of the PLC? TIA Version ? Bye Murof |
Last edited by: Murof at: 03/23/2023 12:06:46If this Information really helps, you could use the Rate function |
|
Follow us on