4/19/2018 9:56 PM | |
Joined: 9/27/2006 Last visit: 5/12/2024 Posts: 12257 Rating: (2666) |
Hello hajar; It seems that the ABB drive FBs for S7 cannot be used with a NPBA adapter: Here is the setup guide for the NPBA as a Profibus-DP slave: https://library.e.abb.com/public/1c08879e220d5acdc2256df100503448/EN_NPBA_12_UM_B.pdf Since this adapter uses Profidrive satandards, the various registers defined in the choice of PPO_ can be accessed directly, one by one (the easiest way, with Move instructions in LAD) or with SFC15 and SFC 14 (DPRD_DAT and DPWR_DAT) with more diffficulty. Hope this helps, Daniel Chartier |
4/20/2018 11:36 PM | |
Posts: 22 Rating: (2) |
i think it can work bcs it the same telegrame |
Follow us on