4/21/2018 8:29 AM | |
Joined: 6/10/2008 Last visit: 8/29/2024 Posts: 191 Rating: (1) |
Hello, I wonder whether is possible to perform simulation with PLCSIM (when actual HW PLC is not present) with PLCSIM v5.4 installen in package STEP 7 professional v5.5? The HMI application is on the PC and is configured to connect to PLC via TCP/IP i.e. Ethernet. When I start PLCSIM, I can only choose PLCSIM(TCP/IP) but there is no option to set up IP address, therefore the communication to HMI is not possible. I have read material here: https://support.industry.siemens.com/cs/us/en/view/109748099 and if I'm not mistaken, I need some advanced PLCSIM software for this task. Any advice is highly appreciated. Thank you! |
Last edited by: Jen_Moderator at: 4/23/2018 11:29:00 AMOptimized link. |
|
5/8/2018 7:21 PM | |
Joined: 6/10/2008 Last visit: 8/29/2024 Posts: 191 Rating: (1) |
Thank you guys. Thomas, can you suggest link for your software? |
9/23/2020 8:37 AM | |
Joined: 3/12/2015 Last visit: 5/31/2024 Posts: 1 Rating: (0) |
Thanks So much, I've ready downloaded and tested. It's so good at all. Thanks again |
Follow us on