4/17/2018 9:48 PM | |
Posts: 2826 Rating: (684) |
Hello.
It will be most helpful if you could be specific to the part number of the analog card you have to use. Or do you use analog on-board to the PLC? See this tip to show how you can get some more information on a specific part: https://support.industry.siemens.com/tf/uk/en/posts/188646/ In the hardware configuration is the declaration of which input address is linked to the analog input. Also there the type of analog (example: -10 .. 10V) can be set - when available. The system manual of the PLC is helpful in showing which number range represents the full range of the analog input. You would get many tips by searching these forum pages for "scaling of analog inputs" or something similar. That is as much as I can help - I am not licensed to use the S7-1500 on my computer. ~ |
4/21/2018 5:39 PM | |
Joined: 5/6/2010 Last visit: 4/24/2024 Posts: 1963 Rating: (272)
|
Hello MyhreN, you use a PLC compact with integrated I/O. For the manual please look at this link - SIMATIC S7-1500 CPU 1512C-1 PN Wiring analog I/O for voltage masurement - you can find informations at page 82 chapter 4.3.2 For programming:
The addresses of the analog inputs you can find at page 114 at chapter 5.1 Hope this is helpful to start your project. If you have more questions, do not hesitate to ask the forum regards |
Last edited by: Jen_Moderator at: 4/23/2018 12:17:09 PMOptimized link. |
|
Follow us on