4/21/2018 11:08 AM | |
Posts: 2826 Rating: (685) |
Hello. I think the description of the "problem" is much too thin and generic. There is not even mention on what the application is. Even the vision sensor is not clear which model in the range it is. Claiming that the PLC configuration is correct does not convince me either - there is no evidence that anything was done from the topic starter side. Perhaps the following page can help for some insight on how to connect the PLC and vision sensor. Maybe it helps you to understand how to help the topic starter. (no sarcasm) https://www.keyence.com/support/user/applicationsensor/download/connections/index.jsp#point1 |
Last edited by: #dP at: 4/21/2018 11:10:01 AM |
|
4/21/2018 8:12 PM | |
Joined: 3/28/2014 Last visit: 9/5/2024 Posts: 82 Rating: (0) |
Thanks, Profinet IO system(100) |
Follow us on