5/18/2018 2:15 PM | |
Joined: 12/12/2008 Last visit: 10/7/2019 Posts: 69 Rating: (6) |
Hi Jan, I am trying to build my image on the jan/rocko branch, and I get following error that I can not resolve: poky/meta/recipes-devtools/gcc/gcc_7.3.bb:do_compile failed with exit code '1' I am building on a vmware, ubuntu 16.04 LTS. Have you encountered this in any way? I have solved other problems, but this one, I have no clue on how to investigate.. Edit: There is also an error on: poky/meta/recipes-devtools/binutils_2.29.1.bb:do_compile. The error log is longer than anything else i`ve seen. Almost everything is "undefined reference to " something. /Benjamin ------------------------------------------------------------------------------------------ |
Last edited by: Ben1902 at: 5/18/2018 2:21:23 PMLast edited by: Jen_Moderator at: 5/18/2018 2:49:19 PMNew subject after splitting |
|
5/19/2018 5:23 PM | |
Joined: 4/28/2015 Last visit: 1/29/2024 Posts: 574 Rating: (43) |
I'm not aware of anyone having tried that with Ubuntu so far. It works fine on my SUSE 42.3, and also in the Debian 9-based kas container (trying the Docker build path might be worthwhile BTW). OTOH, 16.04 is officially listed as "supported" by Yocto (https://www.yoctoproject.org/docs/2.4/ref-manual/ref-manual.html#detailed-supported-distros). Maybe it is an issue related to the vmware setup. Are you building over a shared folder or something like this, or is that build folder a normal Linux filesystem? |
Last edited by: jan-k at: 5/19/2018 5:24:33 PM |
|
Follow us on