5/22/2018 4:26 PM | |
Joined: 8/3/2009 Last visit: 4/23/2024 Posts: 12834 Rating: (1639)
|
Hello It depends which WInCC RT you use: WinCC Professional RT -> yes you can use C Script but the F(x) Trend Control has a VB interface, so you should use VB Script in this case. WinCC Advanced RT-> you can use this FAQ and the F(x) Trend Control: https://support.industry.siemens.com/cs/ww/en/view/109481693 Bye Murof |
If this Information really helps, you could use the Rate function |
|
5/24/2018 8:17 AM | |
Posts: 4 Rating: (0) |
I am using WinCC Professional. |
This contribution was helpful to1 thankful Users |
5/24/2018 8:20 AM | |
Posts: 4 Rating: (0) |
Dear Sir, I want to have XY motion of object and Height animation animation for another object in same work area. So I am unable to use trend. I am using animation for XY. I have Attached a Picture How my Output is expected. In that Obj 1 will move in XY motion. with Two tags ( tag 7 & Tag 8 respectively). Bottom 6 objects will be animation Height with Tag 1 to Tag 8. Values 1 to values 4 will be calculated from tags using C Script and displayed in Screen. How can I get (0,0) to bottom left in XY motion.? How can I use C script to fetch PLC tags as input and after calculation how to get that values as tag for screen.? AttachmentScreen.pdf (122 Downloads) |
Last edited by: AutoGen_2824906 at: 5/24/2018 10:22:37 AM |
|
Follow us on