5/24/2018 7:08 AM | |
Joined: 3/14/2010 Last visit: 2/3/2024 Posts: 359 Rating: (5) |
Hi, Murof ! First I used TIA portal v.13 with WinCC v.13 Comfort / Advanced and everything was Ok. I could get any curve with any style (“dash” or “solid”) in Runtime. But a time scrolling in the “trend view” control object didn’t work in RT and I was forced to install WinCC v.13 Profess where the time scrolling worked Ok. So now I use TIA portal v.13 Profess. (STEP7 v.13 Profess + WinCC v.13 Profess). Both them has initial modification, i.e. there are no updates for STEP7 and for WinCC installed. I don’t use PLCSIM from this package (TIA). The PLC – project was made with migration from old one based on STEP7 v.5.5 +SP4. So I use the old PLCSIM v.5.4 + SP5 + Upd3 After migration I began to develop the HMI-part of the new project for TP1500 Comfort. I have Updates for TIA v.13 :
Can it fix the problem if I install them ? Print screens are attached. AttachmentDash type everywhere.zip (26 Downloads) |
Last edited by: Alex3110 at: 5/24/2018 7:11:42 AM |
|
5/24/2018 12:05 PM | |
Joined: 3/14/2010 Last visit: 2/3/2024 Posts: 359 Rating: (5) |
I have installed the Upd1, but it doesn't help |
6/7/2018 4:02 PM | |
Joined: 8/3/2009 Last visit: 3/27/2024 Posts: 12651 Rating: (1621)
|
Hello Alex you should always work with the latest Update for your Version. SO you have V13 Without Servicepacks you should use latest Update: https://support.industry.siemens.com/cs/ww/en/view/98211132 I would also consider to update to V13 SP1 UPd9 or V13 SP2 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
9/17/2019 11:05 AM | |
Joined: 3/14/2010 Last visit: 2/3/2024 Posts: 359 Rating: (5) |
Wow, I know the answer !!! It’s a bug of TIA v.13 . After U have installed the SP1 for TIA v.13 everything works Ok. |
Follow us on