5/25/2018 12:21 PM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, When the driver block is not inserted automatically, it means the block attribute: "s7_tasklist" is not created. The attributes for blocks can only be changed/edited when the block does not have know how protection. In case of the PCS7AnIn, the attribute is available. Can you check if you have it as well? You can see the attribute list at: Blocks folder/FB number->Right click->Object Properties, column: Attributes. Can you also check the following: Component View->Options->Charts->Chart-based Runtime Group Management-> which option is checked? |
Last edited by: Oreca at: 5/25/2018 12:22:56 PMLast edited by: Oreca at: 5/25/2018 12:28:37 PMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on