5/15/2018 11:35 AM | |
Posts: 16 Rating: (3) |
Can any expert could help me with this query? Need this solution urgently. Regards |
5/18/2018 10:59 AM | |
Posts: 16 Rating: (3) |
Hi, Thank you for the reply. My program is in the external shared drive on a PC. I had configured the shared drive in extdev.ini file. I can access the file on the machine but cannot execute through EXTCALL. So can you please specify how to call the .MPF file using the IP address of the PC. Thank you. |
5/25/2018 5:43 PM | |
Posts: 26 Rating: (2) |
You don't say what version you are using, but here is some documentation I have. Hope it may help you. AttachmentEXTCALLforNetworkDrives.pdf (261 Downloads) |
5/28/2018 4:47 AM | |
Posts: 16 Rating: (3) |
Thank you Bcampbell. Tried to use the sample code which you had sent. The issue is, EXTCALL can work for the first time without any issue. But the subsequent calls fails with 14011. I agree with Txote's point that it's to do with "reload buffer forexecuting from externalwas called as subroutine" Can anyone suggest a way to solve this issue. We need to reload the buffer everytime before we execute EXTCALL. If this could be done, the problem could be solved. Regards, Raghav |
This contribution was helpful to1 thankful Users |
Follow us on