5/22/2018 6:29 PM | |
Joined: 3/5/2015 Last visit: 1/2/2023 Posts: 32 Rating: (0) |
Thanks a lot Mr. Duris, I have been able to simulate all signals via Modsim to my PLC and as of now it working fine. There was a Write_Read bit which I had to set to true to be able to write to coils and it worked. But I have another issue now, I am able simulate with modsim successfully. I am also able to recieve data via Modscan from GE successfully. But when both our system communicate it is not working. I mean there is communication coming and going. I try to check i found my CP is terminating the connection. i see in the status the A0FF error is coming and clearing more or less like a pulse. I found someone having the same issue in the below link,i tried to make the UNIT as 1 still the same problem exists, Please advice Mr. Duris, I have attached the configuration in the attachment. Please kindly help ------------------------------------------------------------------------------------------ AttachmentBinder3.zip (693 Downloads) |
Last edited by: Auto-max at: 5/22/2018 6:49:07 PMLast edited by: Auto-max at: 5/22/2018 8:55:31 PMLast edited by: Auto-max at: 5/22/2018 9:19:24 PMLast edited by: Auto-max at: 5/23/2018 6:58:44 AMLast edited by: Auto-max at: 5/23/2018 7:09:09 AMLast edited by: Jen_Moderator at: 5/23/2018 8:47:31 AMNew subject after splitting |
|
Follow us on