6/11/2018 9:13 PM | |
Joined: 11/11/2017 Last visit: 4/21/2024 Posts: 187 Rating: (4) |
evening i have been tasked of creating a little program for a conveyor system: the conveyor will be using a vsd to start and stop and have a pulse counter on the sprocket that will pulse approx 6 pulses per second and on the count of 21 pulses i need the vsd to stop then after a time carry on until the next 21 pulses (this is because they are placing something on the conveyor) now i i think i have written it correctly, just need someone to look at it and tell if its correct and if not point me in the correct way( dont tell me because i need to learn) please ignore the other parts of the program because that is still being worked on. conveyor details if needed are: Conveyor has a 0.55 kW motor At 50 Hz - 9.5 m/min movement speed The toothed sprocket is 125 mm dia, 15 teeth. Each tooth = 26.2mm track movement per pulse 21 pulses per 550mm index movement Approx. 6 pulse per second thanks Attachmentconveyor v1.0.zip (189 Downloads) |
6/13/2018 8:50 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
The attachment is okay. The lsc file can be opened with LSC V8.1 and V8.2. |
6/13/2018 12:06 PM | |
Joined: 4/18/2017 Last visit: 3/21/2024 Posts: 13 Rating: (0) |
Hi I am also unable to open the attached zip file. It appears to be invalid. Nigel |
6/13/2018 12:24 PM | |
Posts: 1283 Rating: (105) |
Attachmentconveyor v1.0.lsc.zip (191 Downloads) |
6/15/2018 7:38 AM | |
Joined: 4/18/2017 Last visit: 3/21/2024 Posts: 13 Rating: (0) |
Hi personally I think you would be better off in this situation with a more mechanical/reliable solution. i suggest you look at an indexing gearbox. Such as the type in this link. http://www.cdsindexers.com/indexing-oscillating-reciprocating-drives/ip-series.php These are adjustable and will not be affected by a stop being pressed, the motor will also not suffer with undue strain to the continuous speed variations. nigel |
Follow us on