6/22/2018 1:43 PM | |
Joined: 11/6/2017 Last visit: 3/21/2024 Posts: 8 Rating: (0) |
Hello! Anyone test TIA Portal V15 upd2 on Windows 10 build 1709 or 1803? It work ok, without problems? Thanks for answers. BR, Jernej ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/25/2018 9:52:55 AMNew subject after splitting |
|
7/19/2018 2:39 PM | |
Posts: 1 Rating: (0) |
I did not get it installed on Win10 1803. I get always the error message: "Die Datei SIA2.exe hat keine gültige Signatur" Strange ... Simon |
7/19/2018 2:57 PM | |
Posts: 2826 Rating: (684) |
TRANSLATE: |
2/11/2019 2:17 PM | |
Posts: 3 Rating: (0) |
I have Win 10 1803. Seems that it is the problem why I can't connect to PLCs. Not sure yet, but there seems to be others having the same issue. |
Follow us on