7/10/2018 5:58 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (871) |
Motor module MLFB number is 6SL3210-1SB1x-xUA3, e.g. 6SL3210-1SB12-3UA0 It works with 1 phase 230 V AC supply & out put is 3 phase AC. It is useful where 3 phase AC supply is not available, so user can connect 1 phase 230 Volt AC supply to SInamics drive & with 1 FKxxx-xAF21-xxxx motor, can run the machine. HTH. |
Last edited by: PISCEAN 2010 at: 7/10/2018 6:01:52 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on