9/25/2016 7:37 AM | |
Joined: 8/9/2016 Last visit: 4/9/2024 Posts: 4 Rating: (0) |
Jose Manuel Gonzalez
Hi everybody I need some help , because I have a problem with a Simotion D445. The problem is that appear this alarm, and stop all the servos, and we have connected the encoder to a adapter to PILZ PNOZ m1p, and then to a SMC 20 (Siemens) and go to the simotion. Technological alarm TO_Axis_10: Alarm Error 20005 : Device type:1, log. address:740 faulted. (Bit:0, encoder number:0, reason: 0x4h). I don't find which it's the problem that occur this alarm, I hope you can help me with this problem. Thanks and I appreciate your support. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/26/2016 2:33:21 PMNew subject after splitting |
|
9/26/2016 6:05 PM | |
Joined: 8/9/2016 Last visit: 4/9/2024 Posts: 4 Rating: (0) |
And we have a this connection with a SMC 20 and Pilz PNOZ m1p, and is a Absolute Encoder. AttachmentPilz - Simotion D.docx (442 Downloads) |
Follow us on