7/13/2018 1:31 AM | |
Joined: 11/12/2008 Last visit: 4/9/2024 Posts: 179 Rating: (16) |
Hello, 1 - You have to empty the scale belt and make sure no Mechanical stress or belt is losses or tighten too much and put down the analog value in PIW. 2 - put full load on the scale belt and put down the value in PIW and this value shold be input in X_Val and dont care if the value is 27648 or less or more the the benefit of our scale FC1 in the attached example 3- I attached the picture with some equation in general you may need to change the numbers, fore example I made the load area 72 cm you have to change it to 2,5 meters and so on. finally you have to read the Net Works comments carefully and the calculation in the attached picture. Hope I touched your mind . AttachmentProcessC.zip (73 Downloads) |
Last edited by: H.SAPER at: 7/14/2018 12:52:56 AMLast edited by: H.SAPER at: 7/14/2018 12:59:45 AMHASSAN.S POJAILA |
|
Follow us on