7/13/2018 11:58 AM | |
Posts: 7 Rating: (0) |
For me is interesting also how to make push button on the web page with LWE and it to be connected with cursor key C1, C2, C3 or C4 or function key F1,F2, F3 or F4. These keys are outside keys and its can used for start some info or stop alarm or reset the system. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/13/2018 2:28:28 PMNew subject after splitting |
|
7/13/2018 3:07 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33794 Rating: (4199)
|
Take a look at attachment if it is okay for you.
AttachmentLWE_Key_test.zip (559 Downloads) |
Last edited by: ixo65 at: 7/13/2018 3:08:03 PM |
|
This contribution was helpful to2 thankful Users |
10/17/2020 10:48 PM | |
Posts: 1 Rating: (0) |
Another tip to use a "Off delay" instead of a "Pulse Relay". |
Follow us on