7/16/2018 11:21 AM | |
Posts: 41 Rating: (1) |
hello Experts I am trying to use the TCP Fileserver application (Entry ID:109475508,Entry date:03/07/2017) on CPU 1510Sp1PN. The communication is not been established between the CPU and Application. The Local Network Adapter is not displayed on the application window. (192.168.0.25) The outputs 'Ready to send' and 'Done' outputs of the FB TcpClient are TRUE. No errors on the FB. Please help. Relevant Screen shots are attached. AttachmentScreenshots.zip (76 Downloads) |
Last edited by: Jen_Moderator at: 7/16/2018 2:13:44 PMAdded all screenshots as a ZIP-File. |
|
7/17/2018 12:07 PM | |
Posts: 41 Rating: (1) |
Thank You Moderator Experts please help me to resolve this issue |
7/20/2018 9:22 AM | |
Posts: 1368 Rating: (126) |
Hello, this Entry use for example the new TCON https://support.industry.siemens.com/cs/de/de/view/109748872 TCON_IP_V4 is more easier to configure as TCON_PARAM. But you need to change the program in some parts...it this is also possible to do:-) |
Follow us on