7/17/2018 1:00 PM | |
Joined: 3/21/2013 Last visit: 5/10/2024 Posts: 21 Rating: (0) |
Hello, Still no answer on this topic ? Specifically I don't know how to set the "Mode Parameter" It is DWORD but in description is 4 Bits and it's not make sense to use DWORD. Maybe in the HELP is a mistake ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/17/2018 3:06:55 PMNew subject after splitting |
|
7/17/2018 4:49 PM | |
Joined: 7/7/2010 Last visit: 5/10/2024 Posts: 14709 Rating: (2356)
|
Let's assume you have a tag named pMode of type Dword so it meets the requirements of whatever you are passing the mode value to. To set the mode bits: pMode.%X0 := CSV or FSR where CSV = false and FSR = true pMode.%X3 := NoDelims or Delims where NoDelims = false and Delims = true If you are concerned about the other bits, before setting the 2 bits, set pMode := 16#0000_0000. There is for sure a lot of wasted bits, but we have no control over that. Either accept it, ignore it, contact Siemens, or stop using Siemens PLCs (maybe there are other options...).
|
science guy |
|
Follow us on