7/1/2014 11:22 PM | |
Posts: 16 Rating: (0) |
Using the S7CP_200 seems to apply to an S7300 configured with TIA Portal (v11) also. |
9/4/2014 10:09 AM | |
Posts: 43 Rating: (0) |
I succeded to connect into Wonderware using Net2PLC.. |
This contribution was helpful to1 thankful Users |
12/24/2014 2:21 PM | |
Joined: 12/4/2013 Last visit: 8/27/2024 Posts: 6 Rating: (1) |
Hi All, Got this working myself this morning. After many headaches. Used the DASSIDirect V3.0 driver. Was very difficult to setup. The WWClient application was very helpful, you can download from Wonderware when you download the driver. Nothing seemed to work until i ran the WWClient, but i think that is because i had the wrong addesses selected. I have made a small word document detailing my config. IP address are for test system.
AttachmentS71200 to Touch Dev01.zip (2463 Downloads) |
This contribution was helpful to3 thankful Users |
Follow us on