8/14/2018 10:05 AM | |
Posts: 3 Rating: (0) |
Dear all, I have upgraded from TIA V14 to TIA V15 , and now the import of text List .awl files is not working if there is a single error in the .awl file. It says "import has failed" with version 14 (and 13), import was done (with errors warning) even if some variables where unknown. it was then easy to use TIA Step7 editor to identify and correct errors; this is really painfull that Siemens did so much control with V15, .awl file import facility is now useless. if any one has an idea to solve that issue ! Best regards
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/14/2018 11:59:39 AMNew subject after splitting |
|
8/14/2018 4:50 PM | |
Joined: 7/7/2010 Last visit: 4/17/2024 Posts: 14593 Rating: (2347)
|
You need to install TIA Openness from DVD #2, or the 2nd portal install set if you downloaded from this support site.
|
science guy |
|
Follow us on