8/16/2018 8:49 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32888 Rating: (4066)
|
I have created the program times according to your specifications. Start the simulation and let the actual value increase. Output Q1 is permanently on, since it is below 90. If the transition from 89 to 90 now occurs, it came a pulse for output Q1. However, it can not be recognized as an independent pulse since it only acts as an extension of the on-time of Q1. AttachmentKarthikk.zip (161 Downloads) |
This contribution was helpful to1 thankful Users |
8/17/2018 6:25 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32888 Rating: (4066)
|
The new Version.
AttachmentKarthikk_V2.zip (144 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on