8/31/2018 6:23 AM | |
Posts: 1 Rating: (0) |
Hello All, i have a machine upgrade project i'm starting and want to get a buddy check to make sure i'm on the right path, unfortunately my last PLC experience was in college with old allen bradley hardware and we really only every covered the basics. The system i'm looking to upgrade is small and currently controlled by all 240V mechanical relay timers and switches other than the temperature controls which are set with simple on/off control. Here is a list of the current inputs and ouputs Inputs:
Outputs:
Looking at the technical data it originally appeared the LOGO! 12/24RCEo may be my best out of the box option as it offered analog inputs and the output relays would have been sufficient enough to eliminate some if not all external relays. However reading through some more information it sounds like the analog inputs only accept 0-10 volt signals and wouldn't be useful for K type thermocouples. I'm wondering if a LOGO! 230RCE would be better suited for my application. Ultimately i'd like to simplify this setup to keep it as economical and efficient as possible. |
Follow us on