9/5/2018 7:39 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (374)
|
Hi community, at the moment there is a problem with the node-red-contrib-opcua node für node-red. The client node needs a path to the certificates. Unfortunately this path cannot be changed in the current version (0.2.32). The certificates on the IOT are stored in another location. This is how to solve this issue: The certificates on the IOT2000 are located in
The default (unchangeable) path in node-red is
The solution of this problem is to create the folder
under
and copy the existing folder
from
to
Best regards! |
Last edited by: bergmanu at: 1/30/2019 10:07:46 AMtypo Last edited by: bergmanu at: 1/30/2019 10:08:26 AMtypo Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to4 thankful Users |
Follow us on