9/3/2018 7:59 PM | |
Joined: 9/28/2007 Last visit: 2/20/2024 Posts: 234 Rating: (12) |
Dear Experts I am attaching a program and i want to know. when will Q0.0 output will stat and stop. what inputs are required to activate Q0.0.. i also want to know that when will Q0.1 output will activate and deactivate. what inputs are required to activate and deactivate Q0.1.. if there is any chinese experts then it will be so easy to understand.. if any chinese guy translate this programm then it is so helpful for me.. please help me in this regard.. i want to understand the working of Q0.0 and Q0.1.. please help me I just want to use Q0.0 as normal output. when Q0.1 start then Q0.0 set and when Q0.1 stop then Q0.0 stop
AttachmentKhan.zip (249 Downloads) |
Last edited by: mmkhan at: 9/4/2018 12:59:02 PMMuhammad Munir |
|
9/15/2018 5:45 PM | |
Joined: 9/28/2007 Last visit: 2/20/2024 Posts: 234 Rating: (12) |
Dear see attached file |
Muhammad Munir |
|
9/15/2018 7:02 PM | |
Posts: 2826 Rating: (685) |
Dear
The PTO command is what makes the Q0.0 / Q0.1 pulse. The PTO command is not documented in normal documents. The attached might just help. It is a description of the library that is used in the program you are evaluating. Bye. AttachmentMAP_SERV.zip (225 Downloads) |
Last edited by: #dP at: 9/15/2018 7:04:28 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on