9/14/2018 6:03 PM | |
Posts: 29 Rating: (0) |
Hi guys I’m having this issue using tia basic v14 trying to connect to a 1214c dc/dc/dc FW 2.0. I can connect to the device using V11 prof but I have upgraded the software and within the catalogue I have ensured the device is configured to fw2.0 in the project. I can find the device on 5e network and can also ping the ip so the connection is there but it is just saying that the device is incompatible. I am am really very stuck if someone could advice please. thanks alex ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/17/2018 7:26:37 AMNew subject after splitting |
|
9/14/2018 6:06 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33793 Rating: (4197) |
Please don't post twice for the same problem. See also here, 5th reply: |
9/14/2018 8:41 PM | |
Posts: 29 Rating: (0) |
I have posted here as the previous thread has not given the adiquate answers as I had posted in the incorrect thread. apologies for that. |
9/17/2018 7:27 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Connection issue with 1214 dc/dc/dc is published within the conference SIMATIC S7-1200. Best regards, Jen_Moderator |
Follow us on