9/15/2018 1:02 PM | |
Joined: 9/28/2017 Last visit: 11/29/2023 Posts: 64 Rating: (0) |
DEAR ALL, Good day. I am presently working on a project consisting of Siemens s7400h system and Sirius 3wr44 soft starter. the soft starters are all commissioned. now I have to read some data like current, voltage, operating hour etc. the system has y link to convert redundant Profibus network to single network. I have not work on 3wr44 Profibus communication. now can anyone suggest me the procedure to read data from soft starter to H-CPU and write command to the device through y link from the H-CPU. please suggest me elaborately. I have the GSD file. but in the input-output field, there is only 2byte. how can I read all the required data from only 2 bytes. same for the output command. find the attachment containing hardware configuration of the network of H-CPU and soft starter through y link. Thanks in advance. hope to hear from someone expert soon. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/17/2018 11:17:41 AMNew subject after splitting |
|
9/17/2018 11:18 AM | |
Joined: 6/19/2017 Last visit: 5/3/2024 Posts: 8006 Rating: (163) |
Closed cause question posted twice. The second thread with the subject SOFT STARTER 3WR44 PROFIBUS COMMUNICATION WITH S7400H CPU. is published within the conference Industrial Controls. Best regards, Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on