9/18/2018 12:44 PM | |
Joined: 3/27/2012 Last visit: 6/9/2023 Posts: 32 Rating: (10) |
Fast way is in the attachement: scheduler -> trigger = User change it's fast and simple way. User changes will be saved in alarm log. Don't dorget to enable logging for alarm class "system". If you need that to comply with some serious requirements then please see WinCC Audit option. (link) |
Last edited by: Larionov at: 9/18/2018 12:54:28 PM |
|
9/18/2018 5:04 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hey FT82, also you can use the Options PM logon und Audit With best regards |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
9/9/2022 7:33 AM | |
Joined: 8/3/2009 Last visit: 4/24/2024 Posts: 12854 Rating: (1639)
|
Hello Or you use the build in functionality to log with common alarm logging: https://support.industry.siemens.com/cs/de/en/view/109758223 Bye Murof |
If this Information really helps, you could use the Rate function |
|
2/16/2023 7:33 PM | |
Joined: 10/1/2019 Last visit: 7/22/2023 Posts: 1 Rating: (0) |
thank you for sharing |
Follow us on