9/7/2018 1:31 PM | |
Joined: 4/24/2006 Last visit: 4/15/2024 Posts: 8610 Rating: (1146)
|
Hello, Perhaps you can make some screenshots, to make the problem clearer. Best regards, Wizard |
9/7/2018 1:41 PM | |
Posts: 3 Rating: (0) |
There is phisically TP700, i checked it. The company who done the project give me softwere like on images... Thanks for answering. [snip] AttachmentImages (2).zip (270 Downloads) |
Last edited by: kamil4444 at: 9/7/2018 1:44:27 PMLast edited by: Jen_Moderator at: 9/7/2018 1:49:02 PMRemoved links and added files as an attachment. Last edited by: kamil4444 at: 9/7/2018 1:49:51 PMLast edited by: Jen_Moderator at: 9/7/2018 1:54:47 PMRemoved links and added files as an attachment. |
|
9/7/2018 1:49 PM | |
Joined: 4/24/2006 Last visit: 4/15/2024 Posts: 8610 Rating: (1146)
|
Hello, You have the project for TP177B panel. When you have a TP700 Comfort panel, you need to migrate the project. You can not use WinCC flexible to download TP700 Comfort panel. How do you migrate a project integrated in STEP 7 from WinCC flexible to WinCC (TIA Portal)? How do you migrate a WinCC flexible 2008 project to WinCC (TIA Portal)? When there is a TP700 Comfort, there should be a WinCC TIA Portal project. Best regards, Wizard |
9/21/2018 4:49 PM | |
Joined: 3/17/2014 Last visit: 8/18/2023 Posts: 1 Rating: (0) |
Hi Kamil4444, I ran into a similar problem a couple years back, right when TP177b was discontinued. We had a damaged TP177b panel and couldn't get a new one, on Siemens web site stated that the replacement should be the TP700 so we immediately purchased one, hold and behold, it wasn't so simple to migrate the projects, you can only program the TP700 with the TIA portal. We had a Step7 V5.5. software running a S7-400 and migrating the whole project was out of question, after a lot of looking around, I found out the work around. Here are the Steps: 1) Open your WinCC flexible software and chose to copy from Step 7, this will create a separate problem for the HMI; 2) Open TIA Portal and chose to migrate project, migrate only the WinCC Flexible software you copied from Step7 on step 1). 3) After this you can change the HMI to the new model, but first go to set up, you can change how it will behave when migrating to a different size panel. 4) Change the HMI. 5) You will need to insert a Proxy device to the project, and you will need to point it to your Step7 project, this way it will create a proxy PLC, and voila, should be working. Alternatively, you can ask the supplier for the backup of the TP700 software for download directly, since they should have supplied it to you. PS: the steps above are all on the Wizard documentation, they are just a really compact version of it :) Here is a video about the proxy configuration. https://support.industry.siemens.com/cs/streamingvideo/73502293/776 Best Regards, Rogerio |
Follow us on