9/27/2018 2:13 PM | |
Posts: 8 Rating: (0) |
I have developed a simple downtime tracking system using WinCC Advanced V15.The system requires to log the tag values at the end of the shift to the Microsoft SQL Server.I tested on the local machine and it was working fine as per the requirement. But at a client's location.There is one PC station (Central Server) on which the Microsoft SQL server runs & there is another plant PC on which the WinCC Runtime Advanced run.The communication is working fine and the Central server can be able to see the plant PC.But when we are giving commands to log the tag values its not doing it. Can you guys please help me to find the possible causes? I am following this procedure as documented in the documentation:Here.. |
Follow us on