10/1/2018 5:01 PM | |
Joined: 11/19/2015 Last visit: 4/26/2023 Posts: 3 Rating: (1) |
How can I get active interlock bypass to be shown in PCS7 Measuring point browser? see attached picture. PCS7v9.0 |
10/2/2018 2:54 AM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
Hi jens, How about unselect all the other status and select only the "Bypass" state? Hope i answer your question. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
10/2/2018 9:21 AM | |
Posts: 15 Rating: (1) |
Are you using APL block Intlk08? If yes, then for some inexplicable reason bypassed interlocks are shown under "Manipulated value" and NOT under "Bypass"! |
10/3/2018 9:51 AM | |
Joined: 11/19/2015 Last visit: 4/26/2023 Posts: 3 Rating: (1) |
I'm using APL Intlk04. Not shown under manipulated either. PCS7v9.0, with APL V90 |
10/16/2018 8:58 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi jens.risberg, you can use the bypass information bit to switch the interlock signal in bypass. For this in the interlock block the corresponding bypass enable bit BypEn.Inx and the Feature Bit2 separate evaluation for excluded and simulated interlock signals have to set. More Information you can find in the manual "Advanced Process Library (V9.0 SP1)" in the section "Bypassing signals". with regards |
Follow us on