10/1/2018 9:24 AM | |
Joined: 11/2/2008 Last visit: 9/18/2024 Posts: 92 Rating: (1) |
Hello Prof. Frink, PLC CPU is having good values. Even HMI sometimes read all values and complete graph is displayed. If I trigger the script second time complete data is fetched and full graph is displayed. When HMI is reading values PLC is not writing values to the DB. On HMI side acquisition mode is "cyclic in operation" Actually our job cycle is just 1.5 to 2 secs only If I use standard method to display f(x) graph then I will get only 0-1 samples only. VBScript I am using already described in f(x) trend view graph. Best Regards, |
Last edited by: Rockon at: 10/1/2018 9:44:48 AMLast edited by: Rockon at: 10/1/2018 9:45:29 AMLast edited by: Rockon at: 10/2/2018 4:20:42 PMLast edited by: Rockon at: 10/2/2018 4:21:09 PM |
|
Follow us on