10/14/2018 10:33 AM | |
Posts: 6 Rating: (0) |
LOGO! 8.FS4 version 1.81.03 I made a complex program for an heating system in a building. PDC FINAL 25 - At the start retention worked, now not any more on more blocks after a blackout (more times a day). Sometimes, also the log file is not found (and I'm sure log must be wrote)... When download to logo I receive the error: cannot download because the memory of logo is full. but I can download the program and it work. I have on logo also an SD card in status OK. On logo I have Free Memory: bytes = 3284 blocks = 78 rem = 20 But if I manually change the value of B261 - B137 - B092 as sample, after black out I lost the set value and I have the start one. A bug? Some one can explain? I will upload the program. I hope this sample can help other like me to use temperature setting and logo network connection because I need more time to learn and to find sample. Thank you so much for the help AttachmentPDC rete2.zip (60 Downloads) |
Last edited by: reylon at: 10/14/2018 10:35:15 AMLast edited by: reylon at: 10/14/2018 10:36:21 AM |
|
10/14/2018 11:10 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32893 Rating: (4066)
|
Take a look at attachment. Is this the message that you mean? |
This contribution was helpful to1 thankful Users |
10/15/2018 8:42 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32893 Rating: (4066)
|
The error message is new for me. Start a Support Request. |
10/16/2018 10:05 PM | |
Posts: 6 Rating: (0) |
I will do - thank you |
Follow us on