10/17/2018 11:30 AM | |
Joined: 2/4/2015 Last visit: 6/18/2024 Posts: 64 Rating: (0) |
Hi all, We have CPU313C-2DP for metal pouring application. Level 2 gets weight from Schenck controller via Modbus to TCP communication. We need some Digital inputs to be sent to Level2 PC. So connected a CP343-1 and configured it. CP is in Run mode. But in Netpro connection status is showing closed. I am able to ping the remote computer but connection not established. I have not written AGsend/Receive blocks as of now. Kindly help Regards Surendhar M ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/17/2018 1:20:05 PMNew subject after splitting |
|
10/17/2018 2:45 PM | |
Posts: 3093 Rating: (323)
|
Hello, Block library for Modbus/TCP communication via the CP343-1 or CP443-1 Regards, |
Follow us on