10/18/2018 3:35 PM | |
Joined: 8/3/2009 Last visit: 3/27/2024 Posts: 12651 Rating: (1621) |
Hello Med_selmi It should be no problem do connect it. -> Check in the connection in the HMI Project if you use the IPC Adress of the CP but the Slotnumber of teh CPU!! You can also check everything here: https://support.industry.siemens.com/cs/ww/en/view/24109937 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
10/18/2018 5:53 PM | |
Joined: 4/17/2018 Last visit: 2/26/2024 Posts: 262 Rating: (60) |
Hello Murof, I checked everything is OK( connection, ip adress, pg/pc settings), you can see connection in attachment. but I don't know why it's not working?! IS there any configuration missed of CP343-1 lean? We don't need adding function AG_SEND and AG_RECV in user program? |
Last edited by: Med_selmi at: 10/18/2018 5:57:48 PM |
|
Follow us on