3/3/2014 8:56 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello, Take a look: MICROMASTER 4 (MM4), SINAMICS G120 (CU2x0x): Can I operate a single-phase motor with a MM4/G120 converter? |
5/18/2014 9:21 AM | |
Posts: 8946 Rating: (999) |
No No, there are a lot of Inverters available also for single Phase induction Motors as well. Google is your friend. Just one example: Heigl |
This contribution was helpful to4 thankful Users |
10/21/2018 8:17 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Schade, File nicht gefunden |
Last edited by: Kal.A at: 10/21/2018 8:19:34 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on