10/21/2018 10:06 AM | |
Posts: 1 Rating: (0) |
hi there is building project with about 20 decentrize substation.which automation system is recommended? SICAM PAS?PCS7?SIMATIC MANAGER?DESIGO CC with PXC controller? of cource,SCADA ability should be considered and BMS is by siemens Desigo CC please give me hint thanks and regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/22/2018 7:33:26 AMNew subject after splitting |
|
10/22/2018 8:46 AM | |
Joined: 10/9/2007 Last visit: 9/25/2024 Posts: 1249 Rating: (115) |
Hi I believe it depends on what you need, which communication protocols are available, which functionalities etc. For instance, for the protection and Automation Units on the substation you are best suited with Sicam PAS, as it supports all protocols used by such devices, besides retrieving fault records from them. Connection to power meters is also possible. For building Automation perhaps another System may offer other ready-to-use functionalities. All Systems would them communicate to Desigo CC. If necessary, communication between the Systems is also possible
|
Energy Automation products: Sicam, Siprotec, Digsi |
|
Follow us on