11/22/2018 1:05 PM | |
Posts: 5 Rating: (0) |
Sorry, I just checked that is possible to control the PLC through LOGO! BM, however, I need to have the cursor keys and the function keys in my circuit program. Do you know how I should proceed to do this step? Thanks a lot, Beatriz ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/22/2018 2:13:16 PMNew subject after splitting |
|
11/22/2018 2:16 PM | |
Joined: 12/18/2014 Last visit: 9/22/2024 Posts: 33816 Rating: (4201)
|
In attachment an example. To use the cursor keys in web server, you must first click on ESC key. So you enable the function of the cursor keys in the LOGO! program. If you make the check marks by "Both" and "Web Server" in the message text, you can also use the TDE in web server, you must not have a physical TDE. AttachmentMessage_text.zip (169 Downloads) |
11/22/2018 4:10 PM | |
Posts: 5 Rating: (0) |
Thank you so much, I got it! However, what i want is to turn off and on the PLC via web with this control, it's possible? Thanks again for all the help! |
Follow us on