10/19/2018 12:37 PM | |
Joined: 9/21/2012 Last visit: 9/20/2024 Posts: 4147 Rating: (464) |
I'm with #dP, the problems you are having, is because you don't have the latest version of ALM. |
This contribution was helpful to3 thankful Users |
2/5/2019 5:55 PM | |
Joined: 8/12/2016 Last visit: 2/5/2019 Posts: 1 Rating: (0) |
Gents, I have the same problem with version 1809 so I have to install it on Win 7 or change at TIA 15.1?? |
2/6/2019 6:34 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
or you try the actual ALM Version V6 SP1 https://support.industry.siemens.com/cs/ww/en/view/114358 Regards |
This contribution was helpful to1 thankful Users |
6/19/2019 8:50 PM | |
Joined: 4/28/2015 Last visit: 12/6/2023 Posts: 8 Rating: (0) |
I have Windows 10 Pro Build 18362. I haven't seen anyone post that build yet, but I have had installation problems that show up in the installation log for both Portal and Comfort. Does anyone know if Portal & Comfort can run this build of windows? [Tried that 'Compatibility' link (https://support.industry.siemens.com/kompatool/pages/main/index.jsf?sitc=wwdfi10004 ) It's a bust. Some 'addin' fails to load and then it won't do anything. {'addins' in general are a bad technique}] |
6/19/2019 9:03 PM | |
Joined: 7/7/2010 Last visit: 9/19/2024 Posts: 15207 Rating: (2417)
|
V15.1 might have better luck. Are you using V15? Which update is installed? The latest?
|
science guy |
|
Follow us on