12/7/2018 10:04 AM | |
Posts: 32 Rating: (1) |
I'm trying to take an input from the Arduino serial connection and write that to a file on the IoT2020. The code I'm using testing with is bellow The issue I'm having is that the code does not appear to recognize that there is an input and nothing imputed from the serial appears in the file. I even added an LED "notification" to turn on when a new line is detected in the interrupt but it never turns on. This would mean there is something intrinsically flawed in my code. Any help would be great. Thanks K Since I can't post code please look here https://stackoverflow.com/questions/53666125/arduino-uart-to-file-issue |
Last edited by: Kas.Lewis at: 12/7/2018 10:09:17 AMLast edited by: Kas.Lewis at: 12/7/2018 10:10:09 AMLast edited by: Kas.Lewis at: 12/7/2018 10:10:37 AM |
|
Follow us on