8/5/2016 10:12 AM | |
Joined: 12/18/2014 Last visit: 5/12/2024 Posts: 33020 Rating: (4079)
|
Logo 0BA8 communicates with S7-200 protocol. |
This contribution was helpful to1 thankful Users |
8/5/2016 11:41 AM | |
Posts: 5 Rating: (0) |
is the driver s7 communication suite provide with that protocol or i must use OPC ? |
8/5/2016 12:07 PM | |
Joined: 1/30/2006 Last visit: 4/2/2024 Posts: 310 Rating: (57) |
You should use the protocol Suite. You set You acces the Momory of the Logo by adressing DB1. BR. Sven |
BR. Sven |
|
1/27/2018 11:10 AM | |
Posts: 171 Rating: (43) |
|
This contribution was helpful to2 thankful Users |
12/9/2018 12:09 PM | |
Posts: 2 Rating: (0) |
please email me. thanks |
12/10/2018 8:04 AM | |
Posts: 171 Rating: (43) |
you can ask here itself....... |
Follow us on