12/13/2018 8:40 AM | |
Joined: 5/22/2014 Last visit: 6/19/2024 Posts: 18 Rating: (0) |
Hello experts! That's what i did: 1. In TIA PORTAL "Connections" => "Access point" set "S7ONLINE" 2. Set PG/PC interface "PLSSIM.TCPIP.1" 3. Start simulation PLCSIM 4. Start WinCC simulation. But! After downloading WinCC there is no connection! I tried to look at the settings "Communication Settings", but there is no simulator driver. I tried to test the simulation on the WinCC Advanced. All is well. I want to note that after starting the PLCSIM the system starts to work very slowly. For example, WinCC compiles, opens, and runs for more than 15 minutes. Without a simulator it all takes 1 minute. P.S. In attachment screens connection settings AttachmentScreen.zip (428 Downloads) |
Follow us on