12/8/2018 7:11 PM | |
Joined: 6/18/2018 Last visit: 9/10/2024 Posts: 3 Rating: (0) |
Hello, How to install or configure SNMPD package in IOT 2040 ? Best Regards, |
12/10/2018 1:48 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, You can download the sources from here. Make sure you download the net-snmp-5.8.tar.gz File. Transfer it with WinSCP onto the IOT and unzip it with:
Then enter folder and compile the software:
Kind regards! |
12/11/2018 11:01 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, I just noticed SNMP flags are not set in our linux kernel:
I'll get in touch with development, but I think you might have to build a customized IOT-Image with these Flags switched on. Kind regards! |
12/11/2018 2:13 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, So apparently these are just optional kernel flags, the application should run fine on the IOT. If you installed the same sources I mentioned, then it contains snmp and snmpd. Port 161 seems to be occupied by snmp after installation. Try to see if the process is running:
If yes, kill the process with this PID. Run snmpd on port 161 with this test config:
Then open another putty instance and see if you can read out the MIB:
Seems to work fine for me. To run snmpd at startup, check out this post.
Kind regards! |
Last edited by: Fe_lipe at: 12/11/2018 2:14:58 PMtypo |
|
This contribution was helpful to1 thankful Users |
Follow us on