Industry Online Support
Technical Forum
12/11/2018 11:04 PM | |
Posts: 1 Rating: (0) |
Question: I have a Master/Slave parallel interface that is connected via rs465 cable thru cud2 card. Whenever I try to run drive it immediately generates an F044 fault on Master drive but I can disable the Slave drive and run ok. I've checked connections, replaced communication cable, swapped cud1/cud2 cards with spares with no luck. Actually swapped Slave drive and parallel operation ran ok for abou 12hrs. then the same fault returned? Any suggestions? These are 6RA7095 drives. ------------------------------------------------------------------------------------------ |
Last edited by: KEdge at: 12/11/2018 11:06:23 PMLast edited by: KEdge at: 12/11/2018 11:08:57 PMLast edited by: Jen_Moderator at: 12/12/2018 11:41:02 AMNew subject after splitting |
|
12/17/2018 11:39 AM | |
Joined: 8/25/2006 Last visit: 9/24/2024 Posts: 2209 Rating: (278)
|
Hello. What was the fault value of F044 (r047.001 or r949)? |
Follow us on