12/24/2018 11:25 AM | |
Joined: 11/25/2015 Last visit: 2/15/2024 Posts: 52 Rating: (2) |
Just for reference... SIMATIC S7-PLCSIM Advanced V2.0 is not compatible with software controllers. Nevertheless, I've managed to establish a OUC connection between a simulated CPU1518 (using PLCSIM Adv.) and a real CPU 1507S on the IPC using the virtual ethernet adapter from PLCSIM and the virtual switch. For info, PLCSIM Advanced V2.0 is not compatible with Windows 10 v1803 out-of-the-box. There a modification of the security permissions on certain folders in order to be able to use it: LINK Also, on the IPC, both SIMATIC PC Station Ethernet interface and Software CPU Ethernet interface must be on the same network subnet and connected on a switch in order to monitor online and communicate with the other CPU at the same time |
Last edited by: MatLcq at: 12/24/2018 11:26:16 AMLast edited by: MatLcq at: 12/24/2018 11:38:11 AM |
|
Follow us on